Installing AP6335 Wifi on Nibiru (Android)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing AP6335 Wifi on Nibiru (Android)

2,886件の閲覧回数
kak-dela007
Contributor I

Hello!
I have VR-glasses Magicsee M1. Previously, there was a module WIFi AP6212, which supports only 2.4GHz. But I needed 5.8 GHz WiFi.

I decided to install an AP6335 Wifi module similar in form factor.
But I was faced with the fact that the device does not see it (no network is displayed).

Tell me, please, what should I do to make it work?
I'm not a wizard in programming, is there a step-by-step instruction for installing the AP6335 drivers?
Or another option: who could accomplish my task?


Firmware version: 3.50.12
Version Type: VR0040 / 20171207105854

Kernel version: 3.10.0

nibiru @ nibiru # 529
Thu Dec 7 10:58:26 CST 2017

I also requested the firmware on the official website, but it seems they sent me the previous version. Besides, for some reason, she tries to install
"the model does not match"

I will attach it here (link)

I'm not sure I'm writing this post in the correct section, but I found other similar ones in it. A big request to the moderator, put my question in a more appropriate section, if I posted it incorrectly.

タグ(2)
0 件の賞賛
返信
1 返信

2,487件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

The software that you are using does not match with any of our releases. Unfortunately, we cannot help you.

I apologize for the inconveniences.

Best Regards,

Diego.

0 件の賞賛
返信