Install apt in Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install apt in Yocto

Jump to solution
5,027 Views
eugenephua
Contributor III

Hi there, i have managed to get imx6q to boot up using the files in L3.10.53_1.1.0_iMX6QDLS_Bundle. However, the yocto does not have apt command. May i know if anyone have managed to get it working?

Thanks!

Labels (3)
0 Kudos
Reply
1 Solution
3,058 Views
jaymind
Contributor IV

Hello Eugene,

Plz check below link may it will help you....on same community

Regards

Jaymin D

View solution in original post

0 Kudos
Reply
3 Replies
3,059 Views
jaymind
Contributor IV

Hello Eugene,

Plz check below link may it will help you....on same community

Regards

Jaymin D

0 Kudos
Reply
3,058 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello Jaymin D,

Thanks for your contribution to Freescale Community!

Best regards!

/Carlos

0 Kudos
Reply
3,058 Views
eugenephua
Contributor III

Hi Jaymin,

thanks for the info, i managed to load the debian root file system instead :smileyhappy:

0 Kudos
Reply