Install apt in Yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Install apt in Yocto

跳至解决方案
5,029 次查看
eugenephua
Contributor III

Hi there, i have managed to get imx6q to boot up using the files in L3.10.53_1.1.0_iMX6QDLS_Bundle. However, the yocto does not have apt command. May i know if anyone have managed to get it working?

Thanks!

标签 (3)
0 项奖励
回复
1 解答
3,060 次查看
jaymind
Contributor IV

Hello Eugene,

Plz check below link may it will help you....on same community

Regards

Jaymin D

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,061 次查看
jaymind
Contributor IV

Hello Eugene,

Plz check below link may it will help you....on same community

Regards

Jaymin D

0 项奖励
回复
3,060 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hello Jaymin D,

Thanks for your contribution to Freescale Community!

Best regards!

/Carlos

0 项奖励
回复
3,060 次查看
eugenephua
Contributor III

Hi Jaymin,

thanks for the info, i managed to load the debian root file system instead :smileyhappy:

0 项奖励
回复