Install application on Android 11 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Install application on Android 11 BSP

2,493件の閲覧回数
rahmanuh
Contributor III

Hello,

I am new to Android build system and want to install some applications/libraries/software for example iperf and python3 to Android 11. Is there a way to do that like the Yocto approach? Or is there another way?

Thank you in advance,
Rahmanu

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,463件の閲覧回数
rahmanuh
Contributor III

Hello Hector, 

The BSP version is Android 11.0.0_2.6.0 (Linux 5.10.72 kernel).

Best regards,
Rahmanu

0 件の賞賛
返信

2,381件の閲覧回数
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @rahmanuh ,

In order to achieve this, you'd need to consult the Android OS Documentation since it isn't as straightforward as installing these apps/software on a Linux-based system. Please refer to the following link Android OS Source Documentation  |  Android Open Source Project.

Another way to approach this would be installing a terminal emulator on your Android system (although depending on the emulator there could be some compatibility issues and it all depends on what you're trying to achieve with the installed software.

Let me know if this was of any help.

Best regards,
Hector.

0 件の賞賛
返信

2,476件の閲覧回数
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @rahmanuh ,

I understand that you'd like to achieve this in Android 11, but could you let us know the specific BSP version of Android 11 that you'd like to use?

Best regards,
Hector.

0 件の賞賛
返信