Inquiry on FM function for IMX6 platforms

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry on FM function for IMX6 platforms

1,199 Views
lynntan
Contributor I

Hi, I understand that FM is not supported on the IMX6 platforms ( currently using I.MX6UL EVK with LBEH5HMZPC (802.11a/b/g/n/ac + Bluetooth 4.0 + FM Rx) module If there any solution for us to get the command set and the software driver to enable the FM functionality?  Kindly advise.

0 Kudos
Reply
1 Reply

1,155 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lynn

one can try to get vendor support from

http://wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply