Input and output delay time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Input and output delay time

1,647 Views
akihiromaeda
Contributor I

About I.MX6solo,Do the delay from the camera input to display output is less than 1 frame?

Labels (1)
0 Kudos
Reply
4 Replies

1,396 Views
saurabh206
Senior Contributor III

Yes, it can be possible

0 Kudos
Reply

1,396 Views
akihiromaeda
Contributor I

I want to check just in case

Are you the same answer even after the following operations at the simultaneous?

1.Encode camera input  (1280x720P@30Hz) in H.264

2.Encode a mono audio AAC or MP3

3.And record the encoded video and audio to an SD card in MP4

4.And output the encoded video to wireless LAN module with usdhc

Thank you for your answer.

0 Kudos
Reply

1,396 Views
saurabh206
Senior Contributor III

Hi maeda

Please provide more detail.

Which camera and interface you are trying to use?

Saurabh

0 Kudos
Reply

1,396 Views
akihiromaeda
Contributor I

Hi Saurabh

I have assumed two types of camera I / F

[No.1]

camera input :MIPI-CSI2

Dispay output:DISP0_DATA[7:0]

[No2]

camera input:IPU_CSI0_DATA[19:12]

Display output:DISP0_DATA[7:0]←same as No.1

Output are both YCbCR8bit data.

Thank you for your answer.

0 Kudos
Reply