Incorrect SECO FW Version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Incorrect SECO FW Version

4,421 Views
stuartrubin
Contributor III

I am using an iMX8QM-MEK board and making a custom SCU Firmware (scfw_tcm.bin). With the debug monitor enabled, upon boot, I get the following error:

"Incorrect SECO FW Version 2.3.1 (2.5.4 or later required)"

This error should be self evident. Nonetheless, I can't seem to find versions of the SCFW Porting Kit and the SECO firmware (mx8qm-ahab-container.img) with these versions.

Things seem to work, but how would I know that they were not. Or maybe there is some feature that I have not yet used which will break.

I am building the SCFW with imx-scfw-porting-kit-1.3.0.

The SECO firmware (mx8qm-ahab-container.img) was extracted from "firmware-imx-8.1".

Am I doing something wrong or can someone please steer me towards two compatible versions of the SECO firmware and the SCFW kit?

Thank you

Tags (2)
3 Replies

4,133 Views
thomasschaefer
Contributor III

SECO firmware has been moved from firmware-imx into separate container: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-seco-2.5.4.bin 

4,131 Views
joanxie
NXP TechSupport
NXP TechSupport

what bsp version do you use? let me check the version, it seems your version doesn't match, You can get it using Yocto to fetch firmware-imx package or from this link: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/*.bin

0 Kudos
Reply

3,322 Views
Dante
Contributor I

How to use Yocto to get *.bin ,Can you give some detail steps ?

0 Kudos
Reply