Incorrect SECO FW Version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Incorrect SECO FW Version

4,402件の閲覧回数
stuartrubin
Contributor III

I am using an iMX8QM-MEK board and making a custom SCU Firmware (scfw_tcm.bin). With the debug monitor enabled, upon boot, I get the following error:

"Incorrect SECO FW Version 2.3.1 (2.5.4 or later required)"

This error should be self evident. Nonetheless, I can't seem to find versions of the SCFW Porting Kit and the SECO firmware (mx8qm-ahab-container.img) with these versions.

Things seem to work, but how would I know that they were not. Or maybe there is some feature that I have not yet used which will break.

I am building the SCFW with imx-scfw-porting-kit-1.3.0.

The SECO firmware (mx8qm-ahab-container.img) was extracted from "firmware-imx-8.1".

Am I doing something wrong or can someone please steer me towards two compatible versions of the SECO firmware and the SCFW kit?

Thank you

ラベル(1)
タグ(2)
3 返答(返信)

4,114件の閲覧回数
thomasschaefer
Contributor III

SECO firmware has been moved from firmware-imx into separate container: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-seco-2.5.4.bin 

4,112件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what bsp version do you use? let me check the version, it seems your version doesn't match, You can get it using Yocto to fetch firmware-imx package or from this link: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/*.bin

0 件の賞賛
返信

3,303件の閲覧回数
Dante
Contributor I

How to use Yocto to get *.bin ,Can you give some detail steps ?

0 件の賞賛
返信