In Linux Kernel Debugger: how do I access AIPS memory?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In Linux Kernel Debugger: how do I access AIPS memory?

2,232件の閲覧回数
mindchasers
Contributor III

Hello,

I'm just starting to work with the Arm Developer IDE with a DSTREAM attached to my imx 8MQuad Evaluation Kit (EVK). 

I want to dump out memory mapped registers in the AIPS3 space.  How do I determine this address?  Is there an offset defined by a particular register? 

Let's say I want to dump out the registers start at 0x30B8_0000 for CSI2.  

How would I determine this memory address?

Thank you.

0 件の賞賛
返信
1 返信

2,151件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Robert

addresses description can be found in sect.2.1.2 Cortex-A53 Memory Map, Table 2-5. AIPS3 Memory Map

i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信