Imx93 debugging hdmi audio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx93 debugging hdmi audio

ソリューションへジャンプ
465件の閲覧回数
xiang_1001
Contributor III

bsp version: imx-6.6.36-2.1.0.xml

There is a sound card node now, but there is an error when using the command to play. How to change it?

xiang_1001_2-1758773140767.pngxiang_1001_3-1758773188692.png

 

xiang_1001_0-1758772993598.png

 

0 件の賞賛
返信
1 解決策
114件の閲覧回数
xiang_1001
Contributor III
0 件の賞賛
返信
6 返答(返信)
438件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
392件の閲覧回数
xiang_1001
Contributor III

In the link above, there are only a few about spdif configuration. I have the same configuration as it, but the hdmi audio is still not available. Would you please take a look at it?

 

xiang_1001_6-1759204396761.png

xiang_1001_7-1759204408673.png

xiang_1001_8-1759204424695.png

 

 

0 件の賞賛
返信
425件の閲覧回数
xiang_1001
Contributor III

There is no difference between the linked dts and the one I configured.

0 件の賞賛
返信
343件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

sorry for my late response, local team is on holiday from 10/1-10/8, I'm limited to access the mail,  I attach the dts files which are tested by the internal team and work with hdmi audio, you can refer to that, if still failed and you are urgent, you can "submit a ticket" from the link as below, attached your error message and dts files, my other location engineers would continue helping you

NXP Technical Support and Resources for Developers | NXP Semiconductors

 

0 件の賞賛
返信
143件の閲覧回数
xiang_1001
Contributor III

Hdmi audio still doesn't work.
I would like to ask, has nxp tried hdmi audio?
This lt9611 driver can be used on imx8, and it also has audio. However, on imx93, no audio came out, and an error was reported below.

xiang_1001_0-1761211467828.png

 

0 件の賞賛
返信
115件の閲覧回数
xiang_1001
Contributor III
Solved
0 件の賞賛
返信