Imx93 debugging IR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx93 debugging IR

Jump to solution
1,402 Views
xiang_1001
Contributor III

Imx93 debugging IR, the schematic diagram is as follows, support IR? If yes, how to debug?

xiang_1001_0-1761211046559.png

 

xiang_1001_1-1761211088899.png

 

0 Kudos
Reply
1 Solution
1,335 Views
gaurav_sharma
NXP Employee
NXP Employee

@xiang_1001 , Please refer imx8mm that has support for IR. Some time back I had tested it and wrote a technical blog - Enabling Infrared Receiver on iMX8MM EVK - NXP Community

The principle remains the same, that a GPIO will be used for an IR receiver. In the blog, I have mentioned the driver and the dtsi to enable it. you can probably start from there and debug.

View solution in original post

0 Kudos
Reply
3 Replies
1,336 Views
gaurav_sharma
NXP Employee
NXP Employee

@xiang_1001 , Please refer imx8mm that has support for IR. Some time back I had tested it and wrote a technical blog - Enabling Infrared Receiver on iMX8MM EVK - NXP Community

The principle remains the same, that a GPIO will be used for an IR receiver. In the blog, I have mentioned the driver and the dtsi to enable it. you can probably start from there and debug.

0 Kudos
Reply
1,389 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I will confirm it for you, please wait.

0 Kudos
Reply
1,362 Views
xiang_1001
Contributor III

Hello, do you have any results?

0 Kudos
Reply