Imx8 IPU Output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8 IPU Output

3,620 Views
omerbenezra
Contributor I

Hi, 

I'm working in IMX8QM of varicite. 

We are looking to change the ipu output to RGBA.

Where in the kernel source code should be change? 

Thank you

Omer

0 Kudos
Reply
2 Replies

3,517 Views
igorpadykov
NXP Employee
NXP Employee

Hi Omer

i.MX8QM has DPU not IPU, linux driver description can be found in

sect.6.2 Display Overview, sect.6.3.1.3 Source Code Structure

attached Linux Manual.

linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,517 Views
omerbenezra
Contributor I

thank you.

i will check the drivers source.

there is example how to connect dpu output to ldb for lvds output?

0 Kudos
Reply