Imx6ull debugging es8328

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6ull debugging es8328

2,296件の閲覧回数
jieh朱
Contributor III

Hello there

                        I am debugging the es8323 audio chip on imx6ull
               The operating system is linux4.1.15
               The driver is sound/soc/fsl/imx-es8328.c and sound/soc/codecs/es8328.c
               Found that imx-es8328.c requires device tree configuration audmux, but there is no menuy maps on imx6ull
               How should I do it?      

0 件の賞賛
返信
3 返答(返信)

2,089件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX6ULL SoC doesn't include the AUDMUX module. Moreover, there seems to be no pre-built support of the ES8328 audio codec on the i.MX6 platform.

0 件の賞賛
返信

2,089件の閲覧回数
jieh朱
Contributor III

Thank you for your reply

      But this driver is available in sound/soc/fsl/imx-es8328.c and sound/soc/codecs/es8328.c

      So I think imx6ull should support es8328

      and there seems to be no pre-built support of the ES8328 audio codec on the i.MX6 platform. What means?

0 件の賞賛
返信

2,089件の閲覧回数
jieh朱
Contributor III

Has anyone debugged es8323?

0 件の賞賛
返信