Imx6s cannot find spi device in linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Imx6s cannot find spi device in linux

跳至解决方案
6,454 次查看
才俊欧
Contributor III

Hi, My board have 2 gpio device on spi bus 1, but I failed to find them in linux via the command:

dmesg |grep spi            <no return>

ls /dev/spi*                    <ls: cannot access '/dev/spi*': No such file or directory>

ls /dev/mtd*                   <ls: cannot access '/dev/mtd*': No such file or directory>

kernel is linux-imx-4.1.15.

The dts config is as below:

&ecspi1 {
  fsl,spi-num-chipselects = <2>;
  cs-gpios = <&gpio3 19 0>,
                   <&gpio2 30 0>;
  pinctrl-names = "default";
  pinctrl-0 = <&pinctrl_ecspi1>;

 adc: adc108@0 {
    #address-cells = <1>;
    #size-cells = <1>;
    compatible = "adc108";
    spi-max-frequency = <1000000>;
    reg = <0>;
  };

  flash: sst25l@1 {
    #address-cells = <1>;
    #size-cells = <1>;
    compatible = "st,sst25vf016b";
    spi-max-frequency = <20000000>;
    reg = <1>;
  };
};

pinctrl_ecspi1: ecspi1grp {
  fsl,pins = <
    MX6QDL_PAD_EIM_D16__ECSPI1_SCLK 0x0001B0B0 //in old ok
    MX6QDL_PAD_EIM_D17__ECSPI1_MISO 0x0001B0B0 //in old ok
    MX6QDL_PAD_EIM_D18__ECSPI1_MOSI 0x0001B0B0 //in old ok
    MX6QDL_PAD_GPIO_19__ECSPI1_RDY 0x0001B0B0 //in old not defined
    MX6QDL_PAD_EIM_EB2__GPIO2_IO30 0x80000000
    MX6QDL_PAD_EIM_D19__GPIO3_IO19 0x80000000

    //MX6QDL_PAD_EIM_D19__ECSPI1_SS1 0x0001B0B0 //
    //MX6QDL_PAD_EIM_EB2__ECSPI1_SS0 0x0001B0B0 //
  >;
};

The  config is:

CONFIG_UNINLINE_SPIN_UNLOCK=y
CONFIG_MUTEX_SPIN_ON_OWNER=y
CONFIG_RWSEM_SPIN_ON_OWNER=y
CONFIG_LOCK_SPIN_ON_OWNER=y
CONFIG_REGMAP_SPI=y
CONFIG_MTD_SPI_NOR=y
CONFIG_MTD_SPI_NOR_USE_4K_SECTORS=y
CONFIG_SPI_FSL_QUADSPI=y
CONFIG_SPI=y
CONFIG_SPI_MASTER=y
CONFIG_SPI_BITBANG=y
CONFIG_SPI_GPIO=y
CONFIG_SPI_IMX=y
CONFIG_SPI_SPIDEV=y
CONFIG_MFD_MC13XXX_SPI=y
CONFIG_SND_SPI=y
CONFIG_SND_SOC_I2C_AND_SPI=y

Can somebody help me? Thank you!

标签 (3)
标记 (1)
1 解答
5,401 次查看
才俊欧
Contributor III

Thank you! I have already ported it.

The main problem is my carelessness, I did not open the ecspi1 in dts.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
5,401 次查看
fabio_estevam
NXP Employee
NXP Employee

There is no driver for 'adc108' in kernel 4.1.15.

In mainline kernel there is drivers/iio/adc/ti-adc108s102.c and the binding is described at: Documentation/devicetree/bindings/iio/adc/ti-adc108s102.txt

So you should use a newer kernel or backport the mainline driver to 4.1.15.

5,402 次查看
才俊欧
Contributor III

Thank you! I have already ported it.

The main problem is my carelessness, I did not open the ecspi1 in dts.

0 项奖励
回复
5,401 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Joe

seems it is necessary to add "spidev" to dts, as in example

spi loaded at /dev/spidev32765.0? 

Can't add spi to /dev 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,401 次查看
才俊欧
Contributor III

Setting the compatible to be "spidev" is helpful.

But, the main reason is absence of status = "okay";

Anyway, thank you for your quick response!