Imx6q surround view solution.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6q surround view solution.

ソリューションへジャンプ
4,337件の閲覧回数
leima
Contributor III

Hi,

I'm doing a postgraduate project about surround view (2D) on imx6q platform, now I'm working on fisheye camera calibration using opencv, the problem is there is no hardware accelerate support in opencv, the image process is too slow, so I have to use gpu. Since imx6q supports opengl es, openvg and opencl, which one should I use in fisheye camera calibration and later in image stitch?

Best regards.

ラベル(1)
1 解決策
3,601件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lei

please check AN4629 Fast Image Processing with i.MX 6 Series
http://www.nxp.com/assets/documents/data/en/application-notes/AN4629.pdf

and useful links
http://imxcv.blogspot.com.br/2014/02/building-opencv-24x-for-freescales-imx6.html
https://community.freescale.com/docs/DOC-328548

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,601件の閲覧回数
leima
Contributor III

This is what I have done now:

Video Link : 7924 

3,601件の閲覧回数
15203565340
Contributor II

Hi, I‘am doing Surround view on imx6q, but I don't know what to do now. Can you share your proposal? my weixin num is 15203565340, I hope you can contact me.

thanks very much!

0 件の賞賛
返信
3,602件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Lei

please check AN4629 Fast Image Processing with i.MX 6 Series
http://www.nxp.com/assets/documents/data/en/application-notes/AN4629.pdf

and useful links
http://imxcv.blogspot.com.br/2014/02/building-opencv-24x-for-freescales-imx6.html
https://community.freescale.com/docs/DOC-328548

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,601件の閲覧回数
leima
Contributor III

Thanks!

BTW, what's the relationship between g2d and opengl, openvg?

0 件の賞賛
返信