Imx6q boot up issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6q boot up issue

1,283 Views
jack-cap
Contributor III

Hi nxp team

   i have made a board according to imx6q-sabresd. i set switch to 01000010 to serial download mode, and  succeed to download image, uboot and rootfs with mfgtools. But whatever i set switch to any boot up mode, mfgtools always show it's a HID-compliant device, and no any debug message was sent to my PC. When I use nxp release uboot-imx6q.imx,it can boot up normal.my compile uboot file can not boot,I ha change nothing about uboot ,the file between nxp release and my compile is the same size  And i really don't know where is the problem. Can anyone help me?

the download log in attachment

Labels (1)
0 Kudos
Reply
1 Reply

1,191 Views
igorpadykov
NXP Employee
NXP Employee

Hi yingjin 

one can follow attached Chapter 3 Porting U-Boot Porting Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply