Imx6 yocto how to integrerate the kernel module with core image base

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx6 yocto how to integrerate the kernel module with core image base

1,262 次查看
bala955
Contributor I

Hi Team

I am trying to integrate the lm75 driver kernel module in core base image for imx6ull EVK.

The BSP version is 2023.04-r0

I keep the driver source inside the following folder location

 

Iam getting the following error when building the bitbake lm75-mod

 

Following changes i did in local.conf

Screenshot from 2024-01-17 12-12-35.pngScreenshot from 2024-01-17 12-16-01.pngScreenshot from 2024-01-17 12-17-45.png

 

Please help me to fix the issue ASAP

 

0 项奖励
回复
3 回复数

1,233 次查看
bala955
Contributor I

thank you for the information

I have another doubt where can I make a change to downgrade the kernel version from 6.1 to 5. or 4.

in yocto source ?

Please reply

0 项奖励
回复

1,232 次查看
bala955
Contributor I

pleas tell which file to modify to do kernel migration changes and next steps to be done in yocot for imx6

0 项奖励
回复