Imx6 with QT5.9.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx6 with QT5.9.2

3,313 次查看
raghavendrasurp
Contributor II

Hi All,

After running our ui binary on Target board, getting this message :

QStandardPaths: XDG_RUNTIME_DIR not set, defaulting to '/tmp/runtime-root'
QEglFSVivIntegration will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.
If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1
imx-ipuv3 2800000.ipu: WARNING: adapt panel end blank lines
Unable to query physical screen size, defaulting to 100 dpi.
To override, set QT_QPA_EGLFS_PHYSICAL_WIDTH and QT_QPA_EGLFS_PHYSICAL_HEIGHT (in millimeters).

Please give me any solution,

Thanks,

Raghavendra

0 项奖励
回复
1 回复

1,998 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Raghavendra

what bsp used in the case, Qt 5.9 is supported in latest nxp bsps, one can try with Linux 4.9.88_2.0.0 Demo Images

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX6QDLSOLOX&appType=license&location=null&... 

linux-imx - i.MX Linux kernel 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复