Imx6 support SAE-J1939 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx6 support SAE-J1939 ?

ソリューションへジャンプ
2,653件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,


Can i.mx6 support CAN bus SAE-J1939?

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,273件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

yes.

J1939 is a higher-layer protocol based on Controller Area Network (CAN).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,273件の閲覧回数
analogicstechin
Contributor III

Hai chip,

 

     please provide the j1939 device  driver for kernel 4.1.15

WE USING THE HARDWARE :
SOC             : MCIMX6Y2DVM05AA (imx6ull-14x14)
PMIC            : PF3000

Kernel Version  : 4.1.15-2.0.1

Best regards

Rakesh K

0 件の賞賛
返信
2,274件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

yes.

J1939 is a higher-layer protocol based on Controller Area Network (CAN).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信