Imx6 support SAE-J1939 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6 support SAE-J1939 ?

Jump to solution
1,507 Views
weikeng-jimmy
Contributor III

Hi Sir,


Can i.mx6 support CAN bus SAE-J1939?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,127 Views
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

yes.

J1939 is a higher-layer protocol based on Controller Area Network (CAN).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,127 Views
analogicstechin
Contributor III

Hai chip,

 

     please provide the j1939 device  driver for kernel 4.1.15

WE USING THE HARDWARE :
SOC             : MCIMX6Y2DVM05AA (imx6ull-14x14)
PMIC            : PF3000

Kernel Version  : 4.1.15-2.0.1

Best regards

Rakesh K

0 Kudos
Reply
1,128 Views
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

yes.

J1939 is a higher-layer protocol based on Controller Area Network (CAN).

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply