Imx6 default SD Card image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6 default SD Card image

2,727 Views
SumitVaidya
Contributor II

Hi,

 

I bought IMX6 evaluation kit and was able to boot evaluation board with SD Card provided in the package.

After that I tried to put my own u-boot.bin and uImage on the SD Card to verify it boots properly.

 

I get following errors when I boot.

 

In:    serial
Out:   serial
Err:   serial
Net:   got MAC address from IIM: 00:19:b8:00:e9:e9
FEC0 [PRIME]
Hit any key to stop autoboot:  0
Card did not respond to voltage select!
mmc0(part 0) is current device
MMC: block number 0x1 exceeds max(0x0)
** Can't read from device 0 **

** Unable to use mmc 0:1 for fatload **
** Bad partition 1 **
mmc1 is current device
reading /6q_bootscript

** Unable to read "/6q_bootscript" from mmc 1:1 **
Loading file "/6q_bootscript" from mmc device 1:1 (xxb1)
** File not found /6q_bootscript

 

I am looking where can I find this 6q_bootscript file. As I lost the default image on SD card where can I find this?

Is there a way to get that default SD Card image back? I searched on website but did not find any documentation for this.

 

Regards,

Sumit

Tags (1)
0 Kudos
Reply
2 Replies

1,912 Views
Chris86
Contributor II

Hi,

I might be able to send you the necessary file, if you can tell me which development board you are using?

0 Kudos
Reply

1,912 Views
SumitVaidya
Contributor II

Hi Chris,

 

I appreciate your help here. I found another SD card with default root file system from Freescale.

I was able to boot my IMX6 with that.

 

Thanks again for your help.

 

Regards,

Sumit

0 Kudos
Reply