Imx6 Hdmi Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx6 Hdmi Problem

1,422 次查看
emmanuelperea
Contributor III

Hello,

I am using a imx6 dual lite connectore that I made a carry board, It's working fine but I have some hdmi issues. 

I have to connect the imx6 to a monitor that use dvi to hdmi connect. 

In dtb configuration i did:

hdmi_video@020e0000 {
compatible = "fsl,imx6q-hdmi-video";
reg = <0x20e0000 0x1000>;
reg-names = "hdmi_gpr";
interrupts = <0x0 0x73 0x4>;
clocks = <0x2 0x7c 0x2 0x7b 0x2 0x8a>;
clock-names = "hdmi_isfr", "hdmi_iahb", "mipi_core";
status = "okay";
fsl,phy_reg_vlev = <0x294>;
fsl,phy_reg_cksymtx = <0x800d>;
digi,dvi_mode;
};

hdmi_audio@00120000 {
compatible = "fsl,imx6q-hdmi-audio";
clocks = <0x2 0x7c 0x2 0x7b 0x2 0x8a>;
clock-names = "hdmi_isfr", "hdmi_iahb", "mipi_core";
dmas = <0xe 0x2 0x19 0x0>;
dma-names = "tx";
status = "disabled";
linux,phandle = <0x5b>;
phandle = <0x5b>;
};

I have four boards with the same configuration, and I have four iquals monitors. One board works excelent and the others works with some issues, in the screen appears some blue and green pixeles.

I dont use hdmi audio so I desabled it from dtb and I put dvi_mode.

I have to use 1024x768 resolution but this mode is not available so I added in xorg.conf file:

My xorg.conf file is the next:

Section "Device"
                        Identifier "i.MX Accelerated Framebuffer Device"
                        Driver "vivante"
                       Option "fbdev" "/dev/fb0"
                       Option "vivante_fbdev" "/dev/fb0"
                        Option "HWcursor" "false"
EndSection

Section "Monitor"
      Identifier "Monitor"   
      HorizSync 48.3
      VertRefresh 60
EndSection

Section "Screen"
      Identifier "Screen"
      Device "i.MX Accelerated Framebuffer Device"
      Monitor "Monitor"
      DefaultDepth 16
       SubSection "Display"
         Depth 16
         Modes "1024x768"
      EndSubSection
EndSection

Section "InputClass"
      Identifier "calibration"
      MatchProduct "AD7879 TouchScreen"

EndSection
Section "ServerFlags"
Option "BlankTime" "0"
Option "StandbyTime" "0"
Option "SuspendTime" "0"
Option "OffTime" "0"
EndSection

Right now I am changing HorizSync and I chek the changes, around 48.4.

I set extra_bootargs -> extra_bootargs=video=mxcfb0:dev=hdmi,1024x768,if=RGB565,bpp=16

I dont know what more i can do, if someone has some idea i will be grateful.

Thanks.

My kernel version is 4.9.

标记 (4)
0 项奖励
回复
1 回复

1,213 次查看
igorpadykov
NXP Employee
NXP Employee

Hi emmanuel

one can look at dvi issues and workarounds described on

DVI Support on i.MX6 boards - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复