Imx53 boot problem on WEC7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx53 boot problem on WEC7

2,669件の閲覧回数
surjitkumar
Contributor II

     I downloaded the image of the WEC7 from adeneo link and tried to boot the QSB START-R board by following the steps given in “FREESCALE_iMX53_QSB_WEC7_user_guide_V131.pdf”.

I have tried to boot the Start-R board by image "........\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel" by using uSD card by using following commands

 

    cfimager -f D:\UPPSALA\WIN_BSP\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\eboot.nb0 -d H -imx53

cfimager -f D:\UPPSALA\WIN_BSP\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\nk.nb0 -d H -imx53 “

After this command if i insert uSD card in START-R board by connecting the power cable and VGA cable, nothing is visible on VGA.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,249件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may try to write Eboot only and then (after SD booting ) to check if (Eboot) output appears
on (UART) console of the i.MX53 QSB. 

2,249件の閲覧回数
surjitkumar
Contributor II

Hi Yuri,

I am using .....\iMX53QSB_WEC7_BIN_V131\image\START-R\VGAPanel\eboot.nb0 -d H -imx53 -a command  to write on uSD.

and i am getting following message

removable = no

device block size = 512 bytes

device block count = 0x3ad4f0

firmware size = 0x80000 bytes (0x400 blocks)

extra blocks = 1022

Flashing eboot.nb0 at sector 0x2

Writing firmware...

Writing FAT partition...

Writing MBR...

done!

but after making the setup but eboot output not appears on UART.I ma using baud rate as mentioned in doc(115200) and using serial to usb com.

0 件の賞賛
返信

2,249件の閲覧回数
surjitkumar
Contributor II

Thanks yuri...... now i am able to boot the board successfully......

0 件の賞賛
返信