Implement a point and line drawing application based on coordinate points, etc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implement a point and line drawing application based on coordinate points, etc

941 Views
ximenbingmeng
Contributor IV

When equipped with the TP framework, touch coordinates are driven by IIC and interrupt INT notifications are sent to the Input subsystem; Tslib must be combined with the input event event;
If the TP pin is given to the M core and the TP reporting point coordinate data and status are transmitted to the A core, how can tslib be called? First, transfer the app from core A of the dual core communication to the lower layer, and then transfer it to tslib from the upper layer; Can the A core APP of dual core communication be directly mapped to tslib?

Tags (1)
0 Kudos
Reply
1 Reply

921 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi   @ximenbingmeng!

 

We don´t have any documentation about tslib.

 

Best Regards!

Chavira

0 Kudos
Reply