Implement a point and line drawing application based on coordinate points, etc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Implement a point and line drawing application based on coordinate points, etc

943件の閲覧回数
ximenbingmeng
Contributor IV

When equipped with the TP framework, touch coordinates are driven by IIC and interrupt INT notifications are sent to the Input subsystem; Tslib must be combined with the input event event;
If the TP pin is given to the M core and the TP reporting point coordinate data and status are transmitted to the A core, how can tslib be called? First, transfer the app from core A of the dual core communication to the lower layer, and then transfer it to tslib from the upper layer; Can the A core APP of dual core communication be directly mapped to tslib?

タグ(1)
0 件の賞賛
返信
1 返信

923件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi   @ximenbingmeng!

 

We don´t have any documentation about tslib.

 

Best Regards!

Chavira

0 件の賞賛
返信