Image sensor for iMX6Ull

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Image sensor for iMX6Ull

1,453 次查看
paultran
Contributor I

hi

please help to provide what image sensor that iMX6ULL support in case SW (driver, kernel....)

with HW connection will follow CSI IP on eval board. 

our application is camera detect QR code, bard code (like 1D, 2D scanner), so image sensor resolution can be around 1MP. 

Please any experiment about that help to advise 

thanks 

标签 (3)
标记 (3)
0 项奖励
回复
2 回复数

1,268 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Paul

please look on

How to use OV5640 with i.MX 6UltraLite EVK - i.MXDev Blog 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,268 次查看
almaz1c
Contributor III

Hi!

Does OV5640 camera module included in i.MX6UltraLite Evaluation Kit | NXP  ?

If no can someone point me how can I order it please?

0 项奖励
回复