Image problem for imx95

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Image problem for imx95

694 Views
OlivierG
Contributor III

Hi

I created an image for imx95 in full mode.

Once I had the image, to flash the image to an SD card, I ran:

sudo dd if=imx-image-full-imx95-95-19x19-verdin.rootfs.wic of=/dev/sda bs=1M $$ sync

The "root" volume is correct.

But the "boot" volume is incorrect.  Instead of being named "boot," it's named "268 MB volume" and it's empty.

Obviously, this SD card won't boot.

What's the problem?

Is there an existing full imx95 verdin image?

Greetings

Olivier

.

0 Kudos
Reply
5 Replies

340 Views
OlivierG
Contributor III

Hi

I use a IMX 95 verdin toradex A1 (not a B0)

The current Yocto on gitlab is made for B0

i get a prebuild image for A1 , it works

Olivier

0 Kudos
Reply

673 Views
OlivierG
Contributor III

finally the boot volume is present

But the image dos not boot , no log on the debug channel, no screen display

i have a Toradex  IMX95 Verdin EVk 

i build the kernel with

MACHINE=imx95-19x19-verdin

is it right ?

 

Olivier

 

0 Kudos
Reply

665 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @OlivierG 

I hope you are doing very well.

 

Could you please share your part number?

Also, Have you tried flashing the image with UUU tool instead with the direct dd command?

In our BSP we support the Machine imx95-19x19-verdin, so it is correct.

 

Best regards,

Salas.

0 Kudos
Reply

635 Views
OlivierG
Contributor III

Hi

i launch : sudo uuu -lsusb

i get

uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141
 
Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion
==================================================
1:2 MX95 SDPS: 0x1FC9 0x015D 0x0001
 
i launch
sudo uuu -b sd imx-boot-imx95-19x19-verdin-sd.bin-flash_all
 
i get

uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141

Success 0 Failure 1


1:2 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -f imx-boot-imx95-19x19-verdin-sd.bin-flash_all

These commands are launch from a Linux ubuntu 24

Where is the problem ?

 

Olivier

 

0 Kudos
Reply

564 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @OlivierG 

 

Please try with:

$ sudo uuu -b sd_all imx-boot-imx95-19x19-verdin-sd.bin-flash_all <your image.wic>

 

Best regards,

Salas.

0 Kudos
Reply