Image Process using IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Image Process using IMX6

2,337 Views
naveenb
Contributor II

Hi, 

I am using IMX6 quad processor and an Imager to capture the Images and video.

Do i need to use the video codecs as an interface between IMX6 quad processor and Imager or IMX6 Quad processor contains inbuilt codecs.

Can anyone guide from the below image which one would be the right way to process the image.

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply
3 Replies

2,230 Views
igorpadykov
NXP Employee
NXP Employee

Hi Naveen

i.MX6Q allows second option as has VPU module described in

Chapter 69 Video Processing Unit (VPU) i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
also please check presentation on
https://community.freescale.com/docs/DOC-95595

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,230 Views
naveenb
Contributor II

Hi Igor, 

Thanks for the reply so i understood I dont need to use any external video codecs for the Image process.

I need one more clarification from your end.

Actually I am working on Infotainment development and i wanted to know do i need to use any media decoder (To play songs from USB which supports MP3, MP4 format) for the audio processing or this is also inbuilt inside IMX6 processor.

Thanks!

Awaiting to your response.

Naveen.

0 Kudos
Reply

2,230 Views
igorpadykov
NXP Employee
NXP Employee

Hi Naveen

audio codecs (these are software codecs) are included in NXP BSPs provided on

i.MX 6 Series Software and Development Tool|NXP 

Best regards
igor

0 Kudos
Reply