imx6q wifi bing up error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q wifi bing up error

5,418 Views
xiaoliangguan
Contributor I

 我在imx6q (android4.4.2 linux3.0.35)移植wifi模块驱动驱动 (ap6441 芯片组为(bcm43341))

 我的移植工作基本完成,

 现在的问题:进行make clean 后重新编译报错log如下:

target thumb C: libhardware_legacy <= hardware/libhardware_legacy/power/power.c
/bin/bash: -c: line 0: unexpected EOF while looking for matching `"'
/bin/bash: -c: line 1: syntax error: unexpected end of file
make: *** [out/target/product/sabresd_6dq/obj/SHARED_LIBRARIES/libhardware_legacy_intermediates/power/power.o] Error 1
make: *** Waiting for unfinished jobs....
target thumb C: libhardware_legacy <= hardware/libhardware_legacy/uevent/uevent.c
/bin/bash: -c: line 0: unexpected EOF while looking for matching `"'
/bin/bash: -c: line 1: syntax error: unexpected end of file
make: *** [out/target/product/sabresd_6dq/obj/SHARED_LIBRARIES/libhardware_legacy_intermediates/uevent/uevent.o] Error 1    

我发现跟device/fsl/sabresd_6dq/BoardConfig.mk
这个文件有关:

这个文件的修改如下:

#Wifi
BOARD_WLAN_VENDOR := BROADCOM
BOARD_WLAN_DEVICE_REV := BCM43341
#for broadcom BCM43341
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
WPA_SUPPLICANT_VERSION := VER_0_8_X
HOSTAPD_VERSION := VER_0_8_X
BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_bcmdhd
BOARD_HOSTAPD_DRIVER := NL80211
BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_bcmdhd
BOARD_WLAN_DEVICE := bcmdhd
WIFI_DRIVER_FW_PATH_PARAM := "/sys/module/bcmdhd/parameters/firmware_path"
WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/bcmdhd.ko"
WIFI_DRIVER_MODULE_NAME := "bcmdhd"
WIFI_DRIVER_FW_PATH_STA := "system/etc/firmware/fw_bcmdhd.bin"
WIFI_DRIVER_FW_PATH_P2P := "/system/etc/firmware/fw_bcmdhd_p2p.bin"
WIFI_DRIVER_FW_PATH_AP := "/system/etc/firmware/fw_bcmdhd_apsta.bin"
WIFI_DRIVER_MODULE_ARG := "iface_name=eth1 firmware_path=/system/etc/frimware/fw_bcmdhd.bin nvram_path=/system/etc/firmware/nvram.txt"

大家知道什么原因影响造成编译错误,这个文件屏蔽的部分是下面:

#WIFI_TEST_INTERFACE := "sta"
# UNITE is a virtual device support both atheros and realtek wifi(ar6103 and rtl8723as)
#BOARD_WLAN_DEVICE := UNITE
#WPA_SUPPLICANT_VERSION := VER_0_8_UNITE
#TARGET_KERNEL_MODULES := \
# kernel_imx/drivers/net/wireless/rtl8723as/8723as.ko:system/lib/modules/8723as.ko \
# kernel_imx/drivers/net/wireless/rtl8723au/8723au.ko:system/lib/modules/8723au.ko \
# kernel_imx/drivers/bluetooth/rtk_btusb.ko:system/lib/modules/rtk_btusb.ko \
# kernel_imx/net/wireless/cfg80211.ko:system/lib/modules/cfg80211_realtek.ko
#BOARD_WPA_SUPPLICANT_DRIVER := NL80211
#BOARD_HOSTAPD_DRIVER := NL80211

#BOARD_HOSTAPD_PRIVATE_LIB_QCOM := lib_driver_cmd_qcwcn
#BOARD_WPA_SUPPLICANT_PRIVATE_LIB_QCOM := lib_driver_cmd_qcwcn
#BOARD_HOSTAPD_PRIVATE_LIB_RTL := lib_driver_cmd_rtl
#BOARD_WPA_SUPPLICANT_PRIVATE_LIB_RTL := lib_driver_cmd_rtl
#for intel vendor
#ifeq ($(BOARD_WLAN_VENDOR),INTEL)
#BOARD_HOSTAPD_PRIVATE_LIB := private_lib_driver_cmd
#BOARD_WPA_SUPPLICANT_PRIVATE_LIB := private_lib_driver_cmd
#WPA_SUPPLICANT_VERSION := VER_0_8_X
#HOSTAPD_VERSION := VER_0_8_X
#BOARD_WPA_SUPPLICANT_PRIVATE_LIB := private_lib_driver_cmd_intel
#WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/iwlagn.ko"
#WIFI_DRIVER_MODULE_NAME := "iwlagn"
#WIFI_DRIVER_MODULE_PATH ?= auto
#endif

把以前系统带的就是我屏蔽的打开,我添加的部分屏蔽掉就编译没有问题,

大家知道这是什么原因造成的。谢谢

Labels (1)
0 Kudos
Reply
4 Replies

4,447 Views
alamyliu
Contributor I

Android provides only wifi.c, which should be sufficient.

For some reason, Freescale tried to support all Qualcomm (Atheros), Broadcom (bcmdhd), and RealTek chips in one wifi-hal, that's wifi_unite.c (which has some bugs in it --- not solid programming I mean).

With your configuration (without modifying Android.mk), it will compile wifi.c, which I havn't tried.

BOARD_WLAN_DEVICE := bcmdhd

Since Freescale's intension is to bring you to use wifi_unite.c. You could change your configuration back to UNITE.

BOARD_WLAN_DEVICE := UNITE

If you have modified Android.mk to compile wifi_bcm.c, you may just try the following options to give it a try.

  1. change wifi_bcm.c to wifi_unite.c in Android.mk (for the BROADCOM block you added)
  2. just copy wifi_unite.c to wifi_bcm.c
  3. copy wifi.c to wifi_bcm.c (You might have to modify the code, and you have to change some configuration in BoardConfig.mk)

After all, have a comparison of wifi.c & wifi_unite.c then you will know what's going on.

Note: The source code I have is 2016 version, which is newer than the document (2015). Thus, I believe that wifi_bcm.c is removed for some reason.

Good luck~

0 Kudos
Reply

4,447 Views
igorpadykov
NXP Employee
NXP Employee

Hi xiaoliang

please check porting guidelines from

Porting BCM4330/BCM43362 WIFI to Android4.2.2 

and try to obtaing chip driver for that kernel version from

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,448 Views
xiaoliangguan
Contributor I

谢谢你的回复,你提到文档我看过了,现在我缺少里面提到的这个文件wifi/wifi_bcm.c
,你能给我发一份这个wifi_bcm.c这个文件吗?

0 Kudos
Reply

4,448 Views
igorpadykov
NXP Employee
NXP Employee

please apply for additional documentation to vendor support

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

0 Kudos
Reply