If the current yocto support the upper version of opencv 3.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If the current yocto support the upper version of opencv 3.1?

1,009 Views
ningwang
Contributor III

    Hi, I want to know if the current yocto support the upper version of opencv 3.1? How to upgrade the opencv version?

I'm using imx6ul bsp but only support opencv 3.1, but the current dnn model have compatibility issues.

    Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

951 Views
igorpadykov
NXP Employee
NXP Employee

Hi ning

for supported versions one can look at Linux documentation on i.MX Software and Development Tools | NXP 

in particular Release Notes document included in latest  Linux 4.19.35_1.1.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply