If i.MX7 is used with 16bits memory bus width

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

If i.MX7 is used with 16bits memory bus width

ソリューションへジャンプ
1,657件の閲覧回数
george
Senior Contributor II

Dear all,

We use one DDR3L.
DCD for them was generated using Aid Script.
In the test using MCIMX7SABRE, it work fine.

From now on, we will design original PCB.
Is termination required though following pins are not used?

  • DRAM_CS1_B
  • DRAM_SDCKE1
  • DRAM_DATA[16:31]
  • DRAM_SDQS2_P
  • DRAM_SDQS2_N
  • DRAM_SDQS3_P
  • DRAM_SDQS3_N
  • DRAM_DQM2
  • DRAM_DQM3

I think that outputs are NC.
Is Pull-up/down required for inputs, such as DQS?

Best Regards,

George

ラベル(2)
1 解決策
1,455件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  yes, the mentioned unused DRAM signals may be left floating.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
1,456件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  yes, the mentioned unused DRAM signals may be left floating.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,455件の閲覧回数
george
Senior Contributor II

Dear Yuri,

Are these all the pins (DQS is also included) that I showed?

Thanks,

George

0 件の賞賛
返信
1,455件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, all the mentioned signals :

  • DRAM_CS1_B
  • DRAM_SDCKE1
  • DRAM_DATA[16:31]
  • DRAM_SDQS2_P
  • DRAM_SDQS2_N
  • DRAM_SDQS3_P
  • DRAM_SDQS3_N
  • DRAM_DQM2
  • DRAM_DQM3

~Yuri.

1,455件の閲覧回数
george
Senior Contributor II

Thanks.

0 件の賞賛
返信