If i.MX7 is used with 16bits memory bus width

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If i.MX7 is used with 16bits memory bus width

Jump to solution
1,596 Views
george
Senior Contributor II

Dear all,

We use one DDR3L.
DCD for them was generated using Aid Script.
In the test using MCIMX7SABRE, it work fine.

From now on, we will design original PCB.
Is termination required though following pins are not used?

  • DRAM_CS1_B
  • DRAM_SDCKE1
  • DRAM_DATA[16:31]
  • DRAM_SDQS2_P
  • DRAM_SDQS2_N
  • DRAM_SDQS3_P
  • DRAM_SDQS3_N
  • DRAM_DQM2
  • DRAM_DQM3

I think that outputs are NC.
Is Pull-up/down required for inputs, such as DQS?

Best Regards,

George

Labels (2)
1 Solution
1,394 Views
Yuri
NXP Employee
NXP Employee

Hello,

  yes, the mentioned unused DRAM signals may be left floating.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

4 Replies
1,395 Views
Yuri
NXP Employee
NXP Employee

Hello,

  yes, the mentioned unused DRAM signals may be left floating.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,394 Views
george
Senior Contributor II

Dear Yuri,

Are these all the pins (DQS is also included) that I showed?

Thanks,

George

0 Kudos
Reply
1,394 Views
Yuri
NXP Employee
NXP Employee

Yes, all the mentioned signals :

  • DRAM_CS1_B
  • DRAM_SDCKE1
  • DRAM_DATA[16:31]
  • DRAM_SDQS2_P
  • DRAM_SDQS2_N
  • DRAM_SDQS3_P
  • DRAM_SDQS3_N
  • DRAM_DQM2
  • DRAM_DQM3

~Yuri.

1,394 Views
george
Senior Contributor II

Thanks.

0 Kudos
Reply