ISL79987 - Image glitch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISL79987 - Image glitch

1,500 Views
monsteera
Contributor II

I'm working on custom board with iMX8MP and isl79987. imx8mp doesn't support virtual channel and interlaced mode, so using as 1 channel. 

I can get an image from the NTSC camera but it seem like a fault. I made same test with another NTSC camera and the result is similar. 

Here is my command for stream:

$ gst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw,width=720,height=480 ! \
beamdeinterlace ! autovideosink sync=false

beamdeinterlace is for externel deinterlaced IMX8MP De-interleave CSI2 PAL 576i video 

 

Image.jpg

How can I fix this image glitch?

 

0 Kudos
Reply
2 Replies

1,417 Views
cbl
Contributor V

Hello @monsteera,

I am developing with the IMX8M Mini.

I am using the ISL79987 IC and I was not able to add the IC to the device tree.

Could you please help me with this?

Is it possible to share a device tree?

Best regards.

0 Kudos
Reply

1,450 Views
joanxie
NXP TechSupport
NXP TechSupport

mailed to you , pls check it

0 Kudos
Reply