ISL79987 - Image glitch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISL79987 - Image glitch

1,457件の閲覧回数
monsteera
Contributor II

I'm working on custom board with iMX8MP and isl79987. imx8mp doesn't support virtual channel and interlaced mode, so using as 1 channel. 

I can get an image from the NTSC camera but it seem like a fault. I made same test with another NTSC camera and the result is similar. 

Here is my command for stream:

$ gst-launch-1.0 v4l2src device=/dev/video3 ! video/x-raw,width=720,height=480 ! \
beamdeinterlace ! autovideosink sync=false

beamdeinterlace is for externel deinterlaced IMX8MP De-interleave CSI2 PAL 576i video 

 

Image.jpg

How can I fix this image glitch?

 

0 件の賞賛
返信
2 返答(返信)

1,374件の閲覧回数
cbl
Contributor V

Hello @monsteera,

I am developing with the IMX8M Mini.

I am using the ISL79987 IC and I was not able to add the IC to the device tree.

Could you please help me with this?

Is it possible to share a device tree?

Best regards.

0 件の賞賛
返信

1,407件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

mailed to you , pls check it

0 件の賞賛
返信