IPv6 configuration for IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPv6 configuration for IMX6

3,300件の閲覧回数
fabio_poiatti
Contributor III

Hi

I costucted a kernel for IMX6 from Yocto Project.

Now I need to configure my IP using IPv6 instead of IPv4.

What does it mean in term of kernel? How is possible to configure it?

And if the IPv6 features has to be applied on PPP?

Thanks

Fabio

0 件の賞賛
返信
3 返答(返信)

3,278件の閲覧回数
fabio_poiatti
Contributor III

sorry any news?

thanks

0 件の賞賛
返信

3,291件の閲覧回数
fabio_poiatti
Contributor III

Hi

I tried the kernel configuration via

bitbake linux-imx -c menuconfig

I found IPv6 configuration under TCP-IP but not under PPP protocol configuration 

Is it possible to configure and use IPv6 under PPP?

Thanks

Fabio

0 件の賞賛
返信

2,177件の閲覧回数
manu_d
Contributor I
Any Idea guys. After 4 years someone facing same issue.
0 件の賞賛
返信