IPU programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPU programming

2,574件の閲覧回数
dhananajysharma
Contributor II
Hi rogeriopimentel,

I am new bee to IMX6 IPU programming, i have seen your post for IMX6 on github, they are for yocto based, I am using Linux BSP 3.10.17 and i want to capture frame from camera using IMX6 sabre board and want to stream it.

i am interseted to use ipu for capture and converting to YUV420.

when i compiled https://community.freescale.com/  shared code its saying error for mxcfb.h

please help me to understand how to do and start IPU programming and deploying that in IMX6 board,

any help will be highly appreciable.

regards,

ラベル(2)
0 件の賞賛
返信
1 返信

1,957件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dhananajy

also suggest to look at ipu examples in imx-test-3.10.17, mxc_v4l2_test

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.17-1.0.0/

they compile fine, use document Freescale_Yocto_Project_User's_Guide.pdf how

correctly compile it, located in package below

L3.10.17_1.0.2_iMX6QDLS_BUNDLE  : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------