IPU programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPU programming

2,576 Views
dhananajysharma
Contributor II
Hi rogeriopimentel,

I am new bee to IMX6 IPU programming, i have seen your post for IMX6 on github, they are for yocto based, I am using Linux BSP 3.10.17 and i want to capture frame from camera using IMX6 sabre board and want to stream it.

i am interseted to use ipu for capture and converting to YUV420.

when i compiled https://community.freescale.com/  shared code its saying error for mxcfb.h

please help me to understand how to do and start IPU programming and deploying that in IMX6 board,

any help will be highly appreciable.

regards,

Labels (2)
0 Kudos
Reply
1 Reply

1,959 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dhananajy

also suggest to look at ipu examples in imx-test-3.10.17, mxc_v4l2_test

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.10.17-1.0.0/

they compile fine, use document Freescale_Yocto_Project_User's_Guide.pdf how

correctly compile it, located in package below

L3.10.17_1.0.2_iMX6QDLS_BUNDLE  : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------