IPU device tree configuration for imx6ul

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IPU device tree configuration for imx6ul

2,383 次查看
davidzhou
Contributor V

Hi,

I have an imx6ul development board.

I can not find any patch that adds IPU driver into the device tree.
    ipu1: ipu@02400000 {
compatible = "fsl,imx6q-ipu";
...
}


Can you help me make or find a patch  file that is "fsl, imx6ul-ipu" compatible?

Thank you,

David

0 项奖励
回复
3 回复数

2,040 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6UL does not have IPU.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,038 次查看
davidzhou
Contributor V

Hi Yuri,

Thank you for reply.

But I found this information:

i.MX Linux® Reference Manual

Document Number: IMXLXRM

Rev. 0, 03/2016

Chapter 6. IPU

IPU The Image Processing Unit (IPU) is designed to

support video and graphics processing functions and to

interface with video/still image sensors and displays.

The IPU driver is a self-contained driver module in the

Linux kernel. It contains a custom kernel-level API to

manipulate logical channels. A logical channel

represents a complete IPU processing flow. The IPU

driver includes a frame buffer driver, a V4L2 device

driver, and low-level IPU drivers.

Table 2-1. Linux BSP Supported Features (continued)

Image Processing Unit (IPU)

Drivers

i.MX 6Quad,

i.MX 6Dual,

i.MX 6DualLite,

i.MX 6Solo,

i.MX 6UltraLite, //IT IS LISTED HERE

i.MX 7Dual

Regards,

David

0 项奖励
回复

2,038 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Looks like this is misprint in Linux documentation, that i.MX6UL and i.MX7 have IPU.
Use i.MX6UL and i.MX7 Datasheets (Hardware specs) and RMs for correct information,

they are equipped with PXP (instead of IPU).

Regards,

Yuri.

0 项奖励
回复