IPU and dual framebuffer support in imx8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IPU and dual framebuffer support in imx8

1,984 次查看
abrahamlincoln
Contributor I

Hi,

We are using imx6 dual core and we are planning to migrate to imx8qm from imx6 dual 

We are using dual framebuffer for our application development. 

  1. Framebuffer 0 -  we run native OpenGL application to fixed resolution (/dev/fb0)
  2. Framebuffer 1 - we run QT application without GPU acceleration (/dev/fb1)

We use IPU to blend above framebuffer to single frame and render to LVDS. 

We would like to follow same approach in imx8qm, documentation says that imx8 does not support dual framebuffer and IPU. 

 

Any ideas to recreate same architecture in imx8 ?

Thanks,

Abu

 

0 项奖励
回复
3 回复数

1,936 次查看
abrahamlincoln
Contributor I

@joanxie  Thanks for your confirmation 

0 项奖励
回复

1,973 次查看
joanxie
NXP TechSupport
NXP TechSupport

i.mx8qm is totally different from imx6d, and imx8qm doesn't support framebuffer driver anymore, if you need to set dual display, you can use the default demo images to test first, it's not easy to migrate from imx6d directly

1,393 次查看
hhami_2040
Contributor III

Hello@abrahamlincoln 

I need the requirement like your question!!

Can you help me if you have solved your problem??

Hello @joanxie

Thank you for your answer!!

What unit is corespondent IPU I.mx6 at Imx.8??

Best regrade

0 项奖励
回复