IPU CSI0 Testmode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPU CSI0 Testmode

1,495 Views
shricco
Contributor I

Hi everyone.

 

I got the i.mx53 QSB at work to develop a camera module. I am new to the board and I tried to create the chess_board test module but I honestly got stuck. Spend over a week trying to get it to work. :/

Has anyone of you tried the chess_board test? It is described in the developers manual IMX53UG.pdf chapter 20.3.

 

I could really need help with die ipuv3_chess.c file. If someone has already implemented the file I would be glad if him or her could send it to me by mail :)

 

thx in advance :)

 

chris

Labels (1)
0 Kudos
Reply
1 Reply

1,352 Views
hake
NXP Employee
NXP Employee
you can refer to ov3640.c which is a real sample, the doc only guide you to create a camera driver from scratch. you can keep the name and modify the setting in ov3640.c, you can refer to the reference manual to check the which register is for test mode.
0 Kudos
Reply