IPU_CSI0_MUX Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPU_CSI0_MUX Configuration

ソリューションへジャンプ
2,316件の閲覧回数
anjojohn
Contributor IV

Hi all,

I have a mipi sensor connecting to imx6Duallite. I have read the i.MX6SDL Reference Manual and came across IOMUXC_GPR13 bits  0-2 and 3-5 for IPU_CSI0_MUX and IPU_CSI1_MUX. In wand-board i see only the IPU_CSI0 configured. I don't understand how this configuration is done. Could any one please explain whats these terms meant

MIPI CSI0
MIPI CSI1
MIPI CSI2
MIPI CSI3
IPU CSI1

and how to set the virtual channel configuration

タグ(3)
0 件の賞賛
返信
1 解決策
2,105件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following https://community.nxp.com/docs/DOC-94312 

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,105件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Hope the following app note helps.

"MIPI–CSI2 Peripheral on i.MX6 MPUs"

http://www.nxp.com/assets/documents/data/en/application-notes/AN5305.pdf >

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

0 件の賞賛
返信
2,105件の閲覧回数
anjojohn
Contributor IV

Hi Yuri,

Thank you for the document. I understand the IOMUXC_GPR1 for IMX6dual/quad. But i don't understand for imx6solo/dualite. IOMUXC_GPR13 register is confusing. what meant by MIPI CSI0, Route MIPI to IPU1 CSI0 ? If it is that then what is MIPI CSI3 and MIPI CSI2. I didn't see any CSI3 or CSI2 input ports. Also is this IPU CSI1 parallel input selection ?

0 件の賞賛
返信
2,106件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following https://community.nxp.com/docs/DOC-94312 

Regards,

Yuri.

0 件の賞賛
返信