IOS Boot fail while loading the MCIMX6-sdb sabre board.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IOS Boot fail while loading the MCIMX6-sdb sabre board.

1,882 次查看
manoharreddyk
Contributor I

Hi,

 

IOS boot failed while loading the MCIMX6Q-SDB SABRE board. We are getting some error and the system goes for suspend state as shown in the attachment.

Please go through the attached console log and give us idea to come out from this issue.

Thanks in advance.

 

Thanks & Regards,

Manohar Reddy.

Original Attachment has been moved to: MCIMX6Q-SDB.txt.zip

0 项奖励
回复
1 回复

1,695 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Manohar

seems you did not rebuild (ported) image for custom board or used wrong image,

so there are many references in log to non-existent devices

connected on i2c bus (like elan-touch). It is necessary to remove

non-used drivers, also it may be useful to look at attached Porting Guide

document.

Images for Sabre board can be found on below link

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复