IMx 6 usb debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMx 6 usb debugger

1,865 次查看
kalai
Contributor I

hi,

 

  i am using imx6sx sabrese sd board. i need to know about debug using usb without any debugger module.

if any IDE available for debug without debugger

how to run the board without memory card?

 

thanks

kalai

0 项奖励
回复
3 回复数

1,847 次查看
kalai
Contributor I

Hi

Will MCUXpresso IDE supports for I.MX 6 series?

 

Regards,

Kalai

0 项奖励
回复

1,838 次查看
Yuri
NXP Employee
NXP Employee

@kalai 
Hello,

  MCUXpresso IDE does not support i.MX6.

Regards,
Yuri,

0 项奖励
回复

1,859 次查看
Yuri
NXP Employee
NXP Employee

@kalai 
Hello,

We do not have recommendations regarding debug IDE over USB.
Usually JTAG (Lauterbach, ARM DS-5 DSTREAM) is applied.
Customer can try using relatively simple command line application,
such as sdphost. The sdphost tool provides a command line interface
for sending Serial Download Protocol (SDP) commands from the PC host
to NXP i.MX devicesin the serial download mode.

You may look at section 4.2.1 (SDPHost downloads Flashloader image)
of the following app note reagrding example how to use it.

 https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf

 

Regards,
Yuri.

0 项奖励
回复