IMXRT1176 Errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1176 Errors

Jump to solution
10,006 Views
Chethanbg
Contributor III

Hi,

We are using RT1170 MCU for our cluster application.

When we are connecting 7" LCD to our custom board out of 7 boards we are getting unknown errors as attached screenshot in 3 boards(while we are running the code, its going to 'usagefault handler' after some time, the time is not definite)and CPU frequency stops and  it is in hanging condition.Without connecting LCD everything works just fine.

Attached is the MCU ,SDRAM and LCD Schematics for your reference.

Let us know what possibly causing this issue?

 

0 Kudos
Reply
1 Solution
9,912 Views
Chethanbg
Contributor III

Hi @Kan_Li 

We resolved issue .

As per recommendation FlexSPI_DQS pin should be left floating  for 133Mhz.in our custom board we connected  FlexSPI_DQS pin to GPIO function.

We reduced speed to 60Mhz now all the devices are working fine.

Thank you for your support 

Thanks & Regards

Chethan B G 

View solution in original post

0 Kudos
Reply
5 Replies
9,976 Views
Chethanbg
Contributor III

Any update on the ticket?

0 Kudos
Reply
9,969 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Chethanbg ,

 

If you have 7 custom boards, but 3 of them had this issue, I would suspect there might be some soldering issue on those boards, did rest of them behave normally as expected all the time? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
9,962 Views
Chethanbg
Contributor III

Hi,

All 7 boards have same issue but the time duration is different

3 boards are hanging after 20 secs and other 4 boards are hanging after 2 hours

0 Kudos
Reply
9,925 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Chethanbg ,

 

Was the frame buffer for the LCD in a none cache area? If not, please do so and check if the problem is still there.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
9,913 Views
Chethanbg
Contributor III

Hi @Kan_Li 

We resolved issue .

As per recommendation FlexSPI_DQS pin should be left floating  for 133Mhz.in our custom board we connected  FlexSPI_DQS pin to GPIO function.

We reduced speed to 60Mhz now all the devices are working fine.

Thank you for your support 

Thanks & Regards

Chethan B G 

0 Kudos
Reply