IMXRT1170 LCD DISPLAY INTERFACE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1170 LCD DISPLAY INTERFACE

1,823件の閲覧回数
ujwal_kumar_N_L
Contributor III

hi i started exploring rt1170 evk to integrate with embedded wizard i referred the example code which has given mcuxpresso ide 

 

IDE details:

MCUXpresso IDE v11.8.0 [Build 1165] [2023-07-26]

 

example file name: wizard_ew_gui_pulse_oximeter

problems

1)after dumping example code i can see only the backlight on, no images or any color popped up so is there anything needs to be change in the rt1170 evk like any jumper etc..

2) if i want to integrate single push button polling or interrupt  to toggle the LCD display color which file needs to be change 

if still information let me know 

Regards

Ujwal

 

@lcdguru @imx23evklcddriv @michael_imxrt 

 

0 件の賞賛
返信
2 返答(返信)

1,779件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ujwal_kumar_N_L,

Could you please share what you see on the serial terminal when running the example code? The terminal's output can let us know in what part of the initialization process it fails. The "readme.txt" file under the "doc" folder exemplifies what you should see.

If all of the initialization process proceeds successfully, then it is likely an issue with your display. Please make sure you are using one of the supported LCD panel as described on the readme.txt file. The supported panels should be: RK055MHD091, RK055AHD091 or RK055IQH091. Also make sure your 5V power supply works correctly and/or try with a different one if possible.

BR,
Edwin.

0 件の賞賛
返信

1,674件の閲覧回数
ujwal_kumar_N_L
Contributor III

Thank you the issue has been resolved ,the display connector was damaged and the Panel had to be defined as RK055AHD091.
Thank you and regards 

UJWAL KUMAR N L

0 件の賞賛
返信