IMXRT1050 EVKB SEMC Deinit and Reinit causing Imprecise Data Bus Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1050 EVKB SEMC Deinit and Reinit causing Imprecise Data Bus Error

ソリューションへジャンプ
1,790件の閲覧回数
jordanwagner
Contributor I

I've modified the SDK's example for SEMC to touch all 32MB of SDRAM, then call SEMC_Deinit() and BOARD_InitSEMC() again.  This only works a few times before generating a hard fault after the call to Deinit, with the fault code reading IMPRECISERR, Imprecise Data Bus Error (0xe000ed28: 0x00000400).  In order to reproduce the error, it seems that a large amount of RAM must be accessed (more than the ~1KB from the example) and the RAM must be deinitialized and reinitialized more than once.  Is this the correct way to bring the SDRAM down and back up again?  The eventual use case for this is to only use the SDRAM occasionally and to deinitialize between uses to save power.  

for(i = 0; i < 10; i++)
{
  SEMC_SDRAMReadWrite32Bit();

  SEMC_Deinit(SEMC);

  if (BOARD_InitSEMC() != kStatus_Success)
  {
    PRINTF("\r\n SEMC SDRAM Init Failed\r\n");
  }
}

タグ(3)
0 件の賞賛
返信
1 解決策
1,549件の閲覧回数
jordanwagner
Contributor I

Turns out that it was an issue with caching.  Using SCB_InvalidateDCache_by_Addr() before the SEMC_Deinit call fixes the issue.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,550件の閲覧回数
jordanwagner
Contributor I

Turns out that it was an issue with caching.  Using SCB_InvalidateDCache_by_Addr() before the SEMC_Deinit call fixes the issue.

0 件の賞賛
返信