IMXRT1050-EVKB DC Power Jack Part Number?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1050-EVKB DC Power Jack Part Number?

2,214 Views
Matt_sampson
Contributor I

Looking for the part number for J2, the 5V DC barrel jack connector on the IMXRT1050-EVKB schematic. I need to order some barrel jacks and would like a P/N to confirm I have the right sized jack. Haven't found this information on the schematic or in the user guide.

 

 

 

0 Kudos
Reply
3 Replies

2,207 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Matt_sampson ,

   You need to check it in the BOM file, J2, you can find the following information

kerryzhou_0-1661744933339.png

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply

2,202 Views
Matt_sampson
Contributor I

Thanks for sharing. Unfortunately when I search for the part number "DC060024202" I still cannot find this part and therefore don't know what sized plug to buy. There look to be some datasheets but ther are in Chinese. Can you provide a P/N for the mating plug or the size of the plug on the eval board?

 

 

Thanks,

 

Mark

0 Kudos
Reply

2,193 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Matt_sampson ,

   In find the mouser also have this DC plug:

https://www.mouser.com/ProductDetail/Gravitech/CON-SOCJ-2155?qs=fkzBJ5HM%252BdCcpvFQyQZHtA%3D%3D

Size like this:

 

I also compare the size with the MIMXRT1050-EVKB J2, it is the same.

So, you can use it.

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply