IMXRT1021 USB MSC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1021 USB MSC

2,143 Views
371153014
Contributor I

Hi, Buddies.

Now I use IMXRT1021 to create my project, but I encounter a problem.

In the official demo, the MSC class of USB device is using RAM as data source.

I have tried many methods that can not modify data source to external memory, such as SPI Flash.

How can I achieve the desired effect?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,737 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 良杰 顾,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to know more information about your question, so whether you can introduce what you had already done to adapt the official demo, does the official demo come from the SDK library?
Looking forward to your reply.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply