IMXRT and RS-485

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMXRT and RS-485

3,115 次查看
anjalikkrishna
Contributor III

Hi,

 I am using MCUXpresso IDE for programming and debugging the imxrt1050 evk .  My task is to display various data in the GUI based on the serial data received via RS485. Whether RS-485 support is there in the basic SDK for this EVK.

How can I check this?

Thanks & Regards,

Anjali

标记 (3)
0 项奖励
回复
2 回复数

2,779 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anjalik

supported features one can find in attached Release Notes included in software package,

seems this is not supported.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,779 次查看
igorpadykov
NXP Employee
NXP Employee

I have internal  update:

"RS-485 can be built with the UART interface. "

Best regards
igor

0 项奖励
回复