IMX95 is equipped with the GC05A2 camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX95 is equipped with the GC05A2 camera

Jump to solution
819 Views
yrj
Contributor III

HI NXP

         1.I want to debug the GC05A2 now. This camera does not have an ISP. How should I configure it to process through the CPU's ISP after modification?

Labels (1)
0 Kudos
Reply
1 Solution
790 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @yrj!

Unfortunately, the GC05A2 camera is not currently supported in our BSP.

However, if your sensor is compatible with the RAW Bayer format and adheres to the Linux camera subsystem (V4L2/media controller framework), the i.MX 95 Camera Porting Guide (UG10215) can help you develop the appropriate driver for integration with the i.MX95 platform.

 

Best Regards,

Chavira

 

View solution in original post

0 Kudos
Reply
1 Reply
791 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @yrj!

Unfortunately, the GC05A2 camera is not currently supported in our BSP.

However, if your sensor is compatible with the RAW Bayer format and adheres to the Linux camera subsystem (V4L2/media controller framework), the i.MX 95 Camera Porting Guide (UG10215) can help you develop the appropriate driver for integration with the i.MX95 platform.

 

Best Regards,

Chavira

 

0 Kudos
Reply